GANTRY.PL.ERR

GANTRY.PL.ERR is the result of AXIS1.PL.FB – AXIS2.PL.FB when GANTRY.STATE = 2.

If GANTRY.STATE is not equal to 2, then the value of GANTRY.PL.ERR will be 0.

Versions

Action Version Notes
Implemented 02-02-02-000  

General Information

Type Read Only
Description Reads the position error present when the drive is in Gantry Mode
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value N/A
Data Type Float
See Also AXIS#.PL.FB
Stored in Non Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

GANTRY.PL.ERR

300eh

01h

Signed32

Position

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3000

1

3000 (0xbb8)

GANTRY.PL.ERR

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

GANTRY.PL.ERR

3000

Signed32

Read Only

Position

Related Topics

GANTRY.PL.ERRFTHRESH | GANTRY.PL.ERRWTHRESH

Position Loop